Faster, lighter and more efficient aircraft.

Commercially viable space exploration. Mission to Mars. To tackle the challenges of the next decade, the digital twin is the key to predicting the performance of a design in the real world. Simulation helps you discover better designs, faster.

詳細

Generating Performance Improvements

Find out how multidisciplinary simulation and design exploration can help to solve the toughest challenges that the aerospace industry has to offer.

100%

STAR-CCM+ is a multidisciplinary CFD tool that allows you to predict the outcome of design changes on the real world performance of a vehicle, including all of the physics that are liable influence it during its operational life.

Click on an icon to learn more

STAR-CCM+ is fully validated to handle multiple flow regimes, complex geometry and motion, allowing virtual testing of the aerodynamic behavior of the full vehicle, be it aircraft, rotorcraft, uav or spacecraft. The resulting design helps cut down on expensive prototype testing and brings a better aerodynamic design to the market faster.

STAR-CCM+ can help with innovative thermal management of the vehicle by simulating and optimizing the thermal performance of engine, avionics and weapons bay virtually before testing. With its ability to handle hundreds of parts, accurate Conjugate Heat Transfer (CHT) analysis and automated process, STAR-CCM+ helps maximize efficiency, reliability and durability, while minimizing material and manufacturing costs and time to market.

STAR-CCM+ is a single unified tool to model all aspects of aircraft icing: impingement, runback, heat transfer, accretion, and aerodynamics. The benefits include reduced simulation licensing cost, improved productivity with one tool, improved accuracy from coupling and safer designs tested and approved in a shorter time and reduced cost.

STAR-CCM+ helps deliver aircraft with improved passenger comfort and optimized cooling of electronics and systems on board. STAR-CCM+ allows full-scale design optimization of ECS including system and interior designs, aircraft modifications, thermal management of engines, cabin/cockpit ventilation, contaminant transport, ducting and avionics cooling. Meet the certification requirements and keep your aircraft light while maximizing cabin comfort with simulation of individual sub-systems or of the entire system together.

As the demand surges towards greater fuel efficiency, quieter aircrafts, lesser emissions and reduced cost/passenger seat/km, innovation is driving the propulsion systems design of today to deliver these results. Be it basic turbomachinery performance, combustion, rotor/stator interaction, plume analysis or erosion, the physics capabilities of STAR-CCM+ are well suited and validated to cover all these areas.

상세 설명

STAR-CCM+ 및 HEEDS를 사용해 항공 우주 설계를 보다 신속하게 발견하세요.

항공 우주 산업은 시간과 예산에 맞춰 혁신적인 새로운 항공기 프로그램을 제공하는 데 있어서 전례 없는 어려움에 직면하고 있습니다. 다중물리 엔지니어링 시뮬레이션은 이러한 요구를 충족시키고 혁신을 추진하는 데 필수적인 도구입니다.

STAR-CCM +는 제품 수명 동안 영향을 줄 수 있는 모든 물리학을 포함하여 항공기의 실제 성능에 대한 설계 변경 결과를 예측할 수 있는 다중물리 CFD 도구입니다. 특별한 파이프 라인 워크플로우, 시장을 선도하는 전처리, 중첩 격자(Overset) 기술 및 광범위한 정확성 검증을 통해 엔지니어는 설계 변경 사항을 신속하게 평가하여 더 나은 설계를 보다 빠르게 발견 할 수 있습니다.

수 백 가지 디자인 변형에 대한 성능 예측과 지금까지 쉽거나 빠르지 않았던 최고의 성능을 갖기 위한 최적화 작업은 다중 물리 탐색(MDX) 도구 HEEDS가 함께 사용됩니다

기존 고객들은 MDX 방식을 사용하여 설계 프로세스 및 제품 설계를 개선함으로써 막대한 비용을 절감하고 혁신적인 새로운 설계를 시장에 내놓았습니다.

“혁신의 자유”

업계에서 설계 주기 내에 시뮬레이션을 효과적으로 활용하기 위한 핵심은 시뮬레이션의 정확성에 있습니다. 또한, 제품 개발 시간이 일반적으로 수년에 걸쳐 진행되는 산업에서, 최고의 설계를 초기에 식별하여 시험 제작 원형을 줄이면 엄청난 시간과 비용을 절약 할 수 있습니다.

 

STAR-CCM +는 다중 유동 체제에서 정확성을 확인 및 검증하고 강건하고 신속한 열 관리 시뮬레이션 접근법을 제공하고 빙결 시뮬레이션을 위한 유일한 산업 솔루션으로 시뮬레이션 시스템 접근법에 적합합니다. 라이센스와 시스템 간의 링크를 철저하게 지원하는 유연한 클라우드 라이센싱 방식과 전담 기술 지원 엔지니어 모델은 제품 설계에서 MDX의 진정한 가치를 실현하는 데 도움을 줍니다.

ユーザー事例

Don't Just Simulate, Innovate!

See how our customers have been using our products to generate design improvements and stay ahead of the innovation race.