Discover Better Designs, Faster.

Multidisciplinary Design Exploration

To stay ahead in the innovation race, engineers need to be able to quickly predict the outcome of design changes on the real-world performance of their product. Together, multidisciplinary simulation and design exploration help engineers discover better designs, faster.

Learn More

MDX Fundamentals

Find out how multidisciplinary simulation and design exploration can help to solve the toughest challenges that the automotive industry has to offer.

100%

Not all engineering simulation tools are created equal. In order to provide a constant stream of relevant engineering data, simulation software must be able to meet certain key criteria.

Click on an icon to learn more.

Previous Next
Multidisciplinary Simulation
The solution of complex industrial problems requires simulation tools that span a multitude of physical phenomena, which often can only be solved using techniques that cross several engineering disciplines. Real-world engineering problems do not separate themselves into convenient categories such as “aerodynamics”, “hydrodynamics”, “heat transfer” and “solid mechanics”. Only multidisciplinary engineering simulation can capture all of the relevant physics and allow you to predict their influence on the real-world performance of a product.
Previous Next
Design Exploration
Engineering simulation allows engineers to see into the future, predicting the consequence of any design changes on the real-world performance of their products. More than that, simulation gives engineers the opportunity to glimpse “all possible futures,” exploring the performance of a product over the full range of operating conditions that it is likely to face in its working life, rather than just at a handful of carefully chosen “design conditions.”
Previous Next
Affordability
Used effectively, engineering simulation consistently delivers a high return on investment (ROI). It provides far more in terms of reduced development costs and increased product revenue than it costs to implement. In order to be practical in a financial sense, simulation software has to be based around a ‘design-exploration’-friendly model that allows engineers to deploy simulations on as many processors as they can lay their hands on, without having to worry about artificial licensing limits imposed by their software vendor and their finance department.
Previous Next
Dedicated Support
In order to be successful, an engineer should have ready access to a community of simulation experts, and ideally an established relationship with a dedicated support engineer who not only understands the engineer’s problems, but can also access the right expert help whenever needed.
Previous Next
Backed by Experts
An uncomfortable truth about modern engineering is that there really are no easy problems left to solve. In order to design truly innovative products, engineers are often “pushing back the boundaries of the possible”. This is something that is difficult to achieve in isolation, and often requires the assistance of experts from outside of an individual engineer’s immediate personal area of expertise. Our software solutions are backed by an international Engineering Services team that can provide assistance in solving the most difficult problems industry has to offer.
In Depth

Multidisciplinary Design Exploration leads to improved product performance

 

Engineering is a process of continual improvement. Engineers are required to improve products step by step, by making incremental changes that are intended to make the product somehow “better”:  Faster; Stronger; Lighter; More efficient; Less expensive.

Every successful product is the result of many design iterations, each of which improves the performance of the product in some manner. While the amount of improvement delivered by each “design upgrade” is often modest, when stacked together over tens, hundreds, or even thousands of design iterations this process delivers products whose performance in the real world is significantly improved over the original design.

However, for every successfully implemented design improvement, there are many more “failed iterations” that either delivered no improvement in product performance or somehow made it worse. For every hard won improvement in a product, there are an almost infinite number of ways to break it. This is the challenge of engineering: to navigate that infinite tree of potential design improvements, making those choices that improve the product (towards some final goal), and rejecting the far more numerous “wrong choices” that would make it worse.

Historically, those predictions came from hand calculations or from the experimental testing of physical prototypes. Although these approaches delivered some of the greatest technological advances of the modern world, they have some fundamental shortcomings.

The first is that both approaches rely on a large degree of simplification as the engineer is forced to simplify the real-world problem into a form that can easily be formulated or tested.

The second is that the cost of physical testing limits its deployment to a small number of specially chosen “design points” that are not necessarily representative of the full range of operating conditions that the product will experience during its lifetime. Thirdly, experimental testing is usually time-consuming and therefore deployed late in the design process - often only as a confirmation of the final design.

Today engineering simulation provides the most reliable flow of information into the design process. It provides comprehensive predictions that are usually more accurate and always less expensive than experimental testing. Deployed effectively, engineering simulation can be used to improve a product by providing a stream of engineering data to drive the design through multiple iterations.

Engineering simulation allows engineers to see into the future, predicting the consequence of any design changes on the real-world performance of their products. More than that, simulation gives engineers the opportunity to glimpse “all possible futures,” exploring the performance of a product over the full range of operating conditions that it is likely to face in its working life, rather than just at a handful of carefully chosen “design conditions.” 

With minimal effort from the engineer, design exploration algorithms can be used to drive the design through a wide range of parametric design variables, configurations, and operating scenarios. Specifically, by employing numerical optimization technology, the design exploration algorithm can intelligently choose the parameters that are most likely to lead to an improvement. Ultimately, this process results in higher quality and more robust products that exceed customer expectations.

 

Case Studies

Don't Just Simulate, Innovate!

See how our customers have been using MDX to generate design improvements and stay ahead of the innovation race.

News, Videos & Publications